MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12 ODR and Sampling Rate Issue?

Posted on October 11, 2014 at 13:30Hello, If LIS2DH12 ODR is set at 10Hz or 25Hz and if MCU reads its XYZ data with 10Hz rate (before reading, MCU does NOT poll any LIS2DH12 registers� status), is there any issue happened when MCU is reading the XY...

ming by Associate
  • 741 Views
  • 0 replies
  • 0 kudos

pressure sensors & humidity sensors

Posted on October 08, 2014 at 05:21how to integrate ST�s pressure sensors and humidity sensors in Linux/Android systems?   #pressure-humidity-sensors

sc by Associate
  • 1085 Views
  • 1 replies
  • 0 kudos

LPS331AP

Posted on January 10, 2014 at 07:54I can't find a forum about barometric pressure sensor. I hope to know the wake up time of the chip from the power down to ready status for the measurement. I also need to know the measurement and conversion time fo...

hitwch by Associate II
  • 1703 Views
  • 3 replies
  • 0 kudos

LSM330 Bits in Data Output

Posted on October 08, 2014 at 14:09Hello How many bit does the data output of the LSM330 have? I can't find it in the datasheet. The register is 2x8 bit long, but are all bits valid? Regards Daniel #lsm330

meerd1 by Associate II
  • 887 Views
  • 0 replies
  • 0 kudos

LSM303DLHC drdy interrupt

Posted on October 08, 2014 at 09:04 I have a STM32F3-discovery board, and I have set up a little test. It just captures ALL input on GPIO3 and count them by channel. Then every seconds, I have a breakpoint with which I look at the numbers, ...

bifrost by Associate II
  • 1181 Views
  • 0 replies
  • 0 kudos

LIS3DH sensitivity

Posted on September 02, 2014 at 17:05The sensitivity for this accelerometer is listed as 1mg/digit at +/-2g FS.  This brings up a few questions.  First, is a ''digit'' and LSB?? Second, at 16 bits, a LSB would be about 0.06 mg, not 1.0 mg.  There's ...

ECB Land pattern for LIS3DSH?

Posted on September 10, 2014 at 19:17Greetings -The LIS3DSH spec sheet says: ''Land pattern and soldering recommendations are available at www.st.com.''So far, I've not been able to find the info. Could someone please point me in a useful direction?...

characteristics of LPS331AP - Temperature Sensing

Posted on May 22, 2014 at 09:08Is there more detailed spec on the temperature sensing of this part? In the data sheet it states +/- 2C from 0-80C. Is there a range where it is tighter?We are finding that room temp (~25C) we are on the high end +1.4C...

jwu by Associate
  • 1168 Views
  • 1 replies
  • 0 kudos

Noise Characteristics?

Posted on October 04, 2014 at 21:33How can we learn the noise densities for many of ST accelerometers? I am currently using analog LIS344ALH in my design, since it has a low noise density stated in datasheet. If intended to use a digital/SPI interfa...

LSM330DLC problem

Posted on July 17, 2014 at 17:33Hi guys,I'm using the LSM330DLC on a weareable device, but while testing I noticed that while measuring the gravity I get values on Z axis around 1380 counts (0x0564 hex raw data coming from the ic).The configuration ...

matias by Associate
  • 1314 Views
  • 1 replies
  • 0 kudos