MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ASM330LHH: About AN5296 Application note power-up requirement

AN5296Application noteASM330LHH: automotive inertial module digital 3-axis accelerometer and digital 3-axis gyroscope3 Operating modes”To guarantee proper power-off of the device, it is recommended to maintain the duration of the VDD line to GND for ...

ggob by Associate III
  • 181 Views
  • 1 replies
  • 0 kudos

LIS2DH12 acceleration data of even number only

Hi, I am working on the LIS2DH12,  I have a problem to the appearance of acceleration data.  I'm using full scale of +/- 2g and ODR of 400Hz.  When the resolution is either 10-bit or 12-bit, only even number acceleration data is read(all x/y/z axis)....

FFKF_Y by Associate II
  • 366 Views
  • 4 replies
  • 0 kudos

STEVAL-STWINBX1 cloud logging

Hello,I have a requirement to log the data from evaluation board STEVAL-STWINBX1 to cloud. I have created Azure IOT hub and while initiating the cloud logging from the app i was unable to successfully connect to the created IOT Device created in azur...

ODR rate on ISM330DHCXTR

Hello, I'm using (ISM330DHCXTR) accelerometer to calculate the phase difference between two axes to measure the movement of a system. configured ODR at 6.6 KHz and measured the operation frequency of the system which has a 10% error while measuring t...