cancel
Showing results for 
Search instead for 
Did you mean: 

asm330lhhxg1 works at VDD/VDDIO=1.8V but does not work if VDD/VDDIO set to 3.3V

arifkhan
Associate II
 
1 REPLY 1
Federica Bossi
ST Employee

Hi @arifkhan ,

If the ASM330LHHXG1 sensor works correctly at 1.8 V for VDD/VDDIO but fails at 3.3 V, possible causes include:

  • Power supply stability: Check for noise or voltage dips at 3.3 V that might affect the sensor.
  • IO level mismatch: Ensure your MCU or interface logic levels are compatible with the sensor’s VDDIO voltage.
  • Incorrect wiring or configuration: Double-check power pins and decoupling capacitors for the 3.3 V setup.
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.