MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MotionDI_update result is abnormal at special angles

We use STM32F103RG to driver ism330dhcx, and use MotionDI to calculate the pitch and roll angle.Parameters:Frequency: 100HzScale: accelero =2gyro = 250AccKnod Caltype:OneTimeGyrKnod CalType:ContinuousSFKnod output type: ENUWhen the object roll angle ...

which by Associate
  • 524 Views
  • 1 replies
  • 0 kudos

Interface 4 wire spi with ILPS22QS

Hello,I am developing an application that uses 8 ILPS22QS in 3-wire mode and a microcontroller that does not support this mode natively. A shift register is used to control the CS lines and it is working as expected.I tried to go around this problem ...

LSM6DSV32X ODR Accuracy

Good Afternoon,I've been working on migrating from the LSM6DSO32 to the LSM6DSV32X and I notice that neither part specifies ODR Accuracy for normal or low power modes.  Is this information available? Thank you

Looking for Accelerometer

Hi, I am looking for an accelerometer. I wonder if there is any ST MEMS chip that meets my requirements:I don't need very high max G force: 4/8G should be enoughLow power consumptionAble to send trigger, like a GPIO rising or falling signal, when acc...

HDaji.1 by Senior
  • 603 Views
  • 1 replies
  • 0 kudos

LSM6DSL big gyroscope fluctuations on acceleration

Hello, I am using a LSM6DSL sensor and when applying a 2G acceleration without rotating the board, I get very important spikes on the gyroscopes of about -90°/s to +90°/s amplitude.This is very strange. Is this a normal behaviour from this sensor ? A...

lsm9ds1-gyroscope

Hi,I have an application with LSM9DS1 sensor and I expected that when I change LSM9DS1 sensor position from horizontal to vertical value will change but changed only when sensor was moving but after that valus comes almost same for horizontal or vert...

JarekG by Associate
  • 585 Views
  • 1 replies
  • 0 kudos

Resolved! IMU Sensor Fusion Performance

Hi Team,I searched sensor fusion performance information of LSM9DS1TR, LSM6DSO IMUs as below,1. Static Accuracy (Yaw, Pitch, Roll) = ?2. Dynamic Accuracy (Yaw, Pitch, Roll) = ?3. Orientation Settling time = sec?However, I did not find it in the respe...

VB.4 by Associate II
  • 685 Views
  • 1 replies
  • 0 kudos