User Activity

I cannot connect to the ST sensor tile.box when using the ST BLE sensor APP. What should I do?
Hi DearThe 90W small projector I designed now requires ST-LED6001 to drive LED, voltage 24V, current 2A. I could not find the complete design of 24V 2A on the official website, all of them are mA level. Do you have the complete reference design of 24...
We selected the Triac ST# T1635-600G for refrigerator project, to control the compressor (inductive loads). Tested T1635-600G, the heat is very serious when passing 16A current, even using a heat sink temperature is more than 100°C. Therefore, I want...