2024-08-15 02:38 AM
We use STM32F103RG to driver ism330dhcx, and use MotionDI to calculate the pitch and roll angle.
Parameters:
Frequency: 100Hz
Scale: accelero =2
gyro = 250
AccKnod Caltype:OneTime
GyrKnod CalType:Continuous
SFKnod output type: ENU
When the object roll angle is close to 90°, MotionDI calculate value is 150°。When the the object roll angle is less than 84°,MotionDI calculate value is normal。How to solve this problem?