MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about Soldering of LIS2DH12

Posted on December 23, 2016 at 04:42I am a new user of ST’s LIS2DH12. I am confused about the sentence 'Leave “Pin 1 Indicator� unconnected during soldering'. It was in chapter 4.1 Soldering information in datasheet of LIS2DH12. What this sent...

Shuyu Ma by Associate II
  • 1593 Views
  • 2 replies
  • 0 kudos

How PDM_Filter_XX_XX works?

Posted on December 29, 2016 at 15:42I'm trying to connect SPH0641LU4H-1 microphone to STM32F411RE Nucleo board.According to the Wikipedia https://en.wikipedia.org/wiki/Pulse-density_modulation format should represent lowest and highest amplitude as ...

circuit design about LIS2DH12

Posted on December 28, 2016 at 08:23I am designing circuit using LIS2DH12. I want to use the I2c, so I connect Cs to high level, and SA0 to GND. I am not sure if CS should be connected to Vdd, or Vdd_IO. As I understand it, Cs should be connected to...

Shuyu Ma by Associate II
  • 1026 Views
  • 1 replies
  • 0 kudos

HTS221 Reset registers to Default

Posted on December 05, 2016 at 20:44Hi.Sorry for my English.specified in the datasheet If a slave receiver does not acknowledge the slave address (i.e. it is not able to receive because it is performing some real-time function) the data line must be...

Akella by Associate II
  • 701 Views
  • 1 replies
  • 0 kudos

LPS331ap supply voltage

Posted on December 21, 2016 at 20:32Hi,I have connected an FPGA to an LPS331ap, and I can retrieve good data as seen in the oscilloscope, but only if the supply voltage is above 2.4V (I have Vdd and Vdd_io shorted together), rather than the 1.71V qu...

Resolved! Does powering LSM6DS3 off pull down I2C lines?

Posted on December 20, 2016 at 17:32I am using the LSM6DS3 component in a design. I've used the component in the past (and always liked it), but never in this capacity. I am using I2C for communication with 10k pull up resistors and am powering on/o...

what is the exact principle of time of flight technology?

Posted on December 17, 2016 at 06:48Hi, i searched for the exact principle of the time of flight technology in internet but the answer i got was different in different websites. I bought VL53l0X sensor recently and i need the exact principle of TOF ...