MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Glitches with the LSM303DLHC

Posted on January 12, 2017 at 12:50I am using the magnetometer on this device, running at the max ODR of 220Hz. There are occasional (several times a minute) glitches which have the following charateristics:1. The interrupt is significantly delayed....

0690X000006062MQAQ.png

LSM9DS1TR gravity expected output

Posted on January 11, 2017 at 12:27Hi, I am using a LSM9DS1TR, with accelerometer scale set to +-16G.With the device motionless on a table, I read a decimal value of 1360 for the Z axis, and if I flip the board over I read -1360 (give or take a few ...

arthur by Associate
  • 823 Views
  • 1 replies
  • 0 kudos

X-NUCLEO-CCA02M1 Expansion sample program problem

Posted on January 08, 2017 at 07:42I have got a strange problem with X-NUCLEO-CCA02M1 expansion board interfacing with NUCLEO-L476RG. I have followedhttps://my.st.com/content/ccc/resource/sales_and_marketing/presentation/product_presentation/d3/44/d...

LIS2DH12 Double Click Interrupt

Posted on January 04, 2017 at 18:13Hi AllI am having some difficulties in configuring the Double Click Interrupt on the LIS2DH12.After power up, I am doing the following:TEMP_CFG_REG = 0xC0CTRL_REG4 = 0x80CTRL_REG1 = 0x77The above seems to work and ...

LSM6DS3 android drivers

Posted on January 09, 2017 at 11:06oliverbeirne‌Where can I find drivers for LSM6DS3 which can be used with Android 6. Android requires both drivers and HAL. I could not find anything on this site. I had seen  a github repository with ST drivers, ...

Simulation files for LPS22/25/331

Posted on January 05, 2017 at 00:51Are there any spice or cadence files to simulate the lps22h/25h/331ap pressure sensors to co-simulate them with an ASIC?If yes, how does one access them?Thanks

Question about Soldering of LIS2DH12

Posted on December 23, 2016 at 04:42I am a new user of ST’s LIS2DH12. I am confused about the sentence 'Leave “Pin 1 Indicator� unconnected during soldering'. It was in chapter 4.1 Soldering information in datasheet of LIS2DH12. What this sent...

Shuyu Ma by Associate II
  • 1581 Views
  • 2 replies
  • 0 kudos

How PDM_Filter_XX_XX works?

Posted on December 29, 2016 at 15:42I'm trying to connect SPH0641LU4H-1 microphone to STM32F411RE Nucleo board.According to the Wikipedia https://en.wikipedia.org/wiki/Pulse-density_modulation format should represent lowest and highest amplitude as ...