MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

circuit design about LIS2DH12

Posted on December 28, 2016 at 08:23I am designing circuit using LIS2DH12. I want to use the I2c, so I connect Cs to high level, and SA0 to GND. I am not sure if CS should be connected to Vdd, or Vdd_IO. As I understand it, Cs should be connected to...

Shuyu Ma by Associate II
  • 652 Views
  • 1 replies
  • 0 kudos

HTS221 Reset registers to Default

Posted on December 05, 2016 at 20:44Hi.Sorry for my English.specified in the datasheet If a slave receiver does not acknowledge the slave address (i.e. it is not able to receive because it is performing some real-time function) the data line must be...

Akella by Associate II
  • 557 Views
  • 1 replies
  • 0 kudos

LPS331ap supply voltage

Posted on December 21, 2016 at 20:32Hi,I have connected an FPGA to an LPS331ap, and I can retrieve good data as seen in the oscilloscope, but only if the supply voltage is above 2.4V (I have Vdd and Vdd_io shorted together), rather than the 1.71V qu...

Resolved! Does powering LSM6DS3 off pull down I2C lines?

Posted on December 20, 2016 at 17:32I am using the LSM6DS3 component in a design. I've used the component in the past (and always liked it), but never in this capacity. I am using I2C for communication with 10k pull up resistors and am powering on/o...

what is the exact principle of time of flight technology?

Posted on December 17, 2016 at 06:48Hi, i searched for the exact principle of the time of flight technology in internet but the answer i got was different in different websites. I bought VL53l0X sensor recently and i need the exact principle of TOF ...

Resolved! IIS2DH interrupt generation and tech details

Posted on November 04, 2016 at 15:57Hi,I would like to use IIS2DH accelerometer as main accelerometer in a custom board for my project. For this reason I've bought the STEVAL-MK1168V1 to make some tests. I would like to ask you some questions about ...

Why is there no self-test function of the magnetometer in LSM303D?

Posted on December 15, 2016 at 10:23Hi there,   According to the datasheet of LSM303D, I could find the self-test function of the accelerometer, but could not find the same function of the magnetometer.   How to test the magnetometer if no build-in ...

looeyc by Associate II
  • 533 Views
  • 1 replies
  • 0 kudos

Resolved! Test LSM6DS3 interrupt with Self Test

Posted on December 15, 2016 at 16:25Hi Everybody, I want to test the interrupt of the LSM6DS3 sensor without any movement. Do you know if it is possible to generate an interrupt with the sensor self test ?If I program a low interrupt threshold and I...

Jerome V by Associate II
  • 1126 Views
  • 5 replies
  • 0 kudos