MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! schizophrenic LIS3DS0

Posted on November 28, 2016 at 17:59Hi everybody,We are using LIS3DS0 on the ISK01A1 board monted on a Nucleo F103-RB...Our software is based on HAL drivers (got in the cube).We met this strange issue in some of our boards (we confirmed the test wit...

samuel23 by Associate III
  • 949 Views
  • 6 replies
  • 0 kudos

SPI COMMUNICATION NOT WORKING

Posted on November 02, 2016 at 23:14Hello Everyone,I am having trouble talking to the LSM6DS3 using 4 wire SPI. I have verified the signals to the device as being correct per the datasheet. I am commanding 0x8F to do a WHO_AM_I command but am not se...

kyle2 by Associate
  • 985 Views
  • 3 replies
  • 0 kudos

LSM6DS3 interrupt pin not going back to low state

Posted on August 10, 2016 at 06:08I brought STEVAL-MKI160V1 MEMS sensor board. Bulk ID Z5T42380E024. While working with the sensor I got an issue like I enabled interrupt generation to interrupt pin INT1 for 6D orientation detection. So when ever I ...

n239955 by Associate
  • 586 Views
  • 1 replies
  • 0 kudos

About LSM330 Register Problem

Posted on February 26, 2014 at 03:15Currently, I am now using LSM330, the only reference driver I found is official Linux-OS driver. Since there's no programming guides, I search website for source code for reference, only to find that all source co...

leo2010 by Associate
  • 628 Views
  • 1 replies
  • 0 kudos

Data Ready Interrupt H3LIS331DL

Posted on February 04, 2014 at 08:30How does one configure the data ready interrupt on the H3LIS331DL accelerometer? I've configured other accelerometers like LIS3DSH with success but I am stuck on this one.I've tried both latched and pulsed interru...

dmg0048 by Associate II
  • 1159 Views
  • 3 replies
  • 0 kudos

lsm6ds3 drivers

Posted on December 12, 2016 at 14:54Can somebody share linux device drivers for kernel 3.7.6 drivers for lsm6ds3

lps22hb no pressure and temperature response

Posted on December 11, 2016 at 07:25I have connected LPS22HB development kit (STEVAL-MET001V1) and Raspberry Pi 3 with I2C interface and tried to read pressure and temperature data but whatever setting I tried, pressure (0x28, 0x29, 0x2A) and temper...

Free-fall and motion detection simultaneously on LIS3DH

Posted on November 29, 2016 at 23:46Hi support,We wonder if there is any register configuration that allow us to route the motion detection to the INT1 pin and the free-fall detection to the INT2 pin and both working at the same time? Both pins are ...

jgaldana by Associate II
  • 770 Views
  • 1 replies
  • 0 kudos

LIS3DHTR data length

Posted on November 02, 2016 at 07:41What is the actual data (x,y,z) length. When I'm reading the acceleration data , the lowest 4 bitsare 0. This would indicate the data is actually 12bit , left justified. The datasheet however say's the FIFO is 10b...

Rob1 by Associate II
  • 746 Views
  • 2 replies
  • 0 kudos