User Activity

[VERSION]: MCWB v6.3.2[TOOL]: STM32CubeMX v6.13.0, STM32CubeIDE v1.11.5[BOARD]: STEVAL-PTOOL1V1[PROJECT]: STEVAL-PTOOL1V1_6S_SLI've been trying to get this board working with a small BLDC motor but the keeps shutting off the motor output when the spe...
I'm testing a STEVAL-PTOOL1V1 board, and I loaded the STEVAL-PTOOL1V1_6S_SL sample project in Motor Control Workbench v6.3.2.  I generated the code (which used STM32CubeMX v 6.13.0) for STM32CubeIDE v1.11.5 toolchain, and the resulting code compiled ...
Posted on September 05, 2017 at 00:08The datasheet shows that setting the D4D_EN bit to 0 enables 4D orientation detection, however in AN5040 in section 5.4.2 it states the opposite.  Also at the end of section 5.4.1 it shows steps to enable 6D dete...
Posted on August 26, 2017 at 01:46I'm trying to configure an LSM6DSL device to provide the wrist tilt interrupt on INT2 and the inactivity interrupt on INT1.  The tilt interrupt appears to work fine.  With inactivity however, I see the interrupt whe...
Kudos from
Kudos given to