MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! H3LIS200DL - Configuration and Readings

Posted on September 02, 2017 at 22:41Hello:I have been fighting with this accelerometer for a couple of months and it has now become imperative that I get it functioning.I am using it with an STM32F405 controller. I have it set up in interrupt mode....

Resolved! LSM6DSL - Clarify D4D_EN bit function

Posted on September 05, 2017 at 00:08The datasheet shows that setting the D4D_EN bit to 0 enables 4D orientation detection, however in AN5040 in section 5.4.2 it states the opposite.  Also at the end of section 5.4.1 it shows steps to enable 6D dete...

LSM303AH - DRDY flag in STATUS_A register

Posted on July 21, 2017 at 16:06The DRDY flag in the STATUS_A register does not seem to work. I am running the acellerometer at ODR =  100Hz, FIFO bypass mode, HR mode. Every time the STATUS_A register is read it outputs the value 65, the DRDY is th...

LIS3MDL single measurement mode

Posted on June 12, 2017 at 12:08Hello, I would like to use the LIS3MDL magnetometer in single measurement mode to reduce my overall current consumption.I've found some useful informations in the AN4602 Application but I'm still missing something.The...

LSM9Ds1 Self-test

Posted on January 12, 2016 at 13:15How may i know about self-test, what is the procedure after enable self-test for each one, and what kind of data will there that i have to use for further analysis, and how. #self-test

bhavesh by Associate II
  • 2303 Views
  • 4 replies
  • 0 kudos

lsm9ds1 self test

Posted on July 31, 2017 at 12:56Hello, I want to do a self test to lsm9ds1.Is there any file that explain how to do it?I found some sources  but nothing official.If there is not official file, i have some questions:Is the sensor can't be in motion a...

4D/6D threshold setting for LIS2DS12

Posted on July 07, 2017 at 02:25Dear sir/madam,I'm confused how the Threshold decodeing(degrees) comes like shown in LIS2DS12 datasheet, page 31. When 6 stands for 80 degrees and how 6 comes from?I try to use 60 degrees threshold and I can read accu...

0690X00000603kIQAQ.jpg

LIS3MDL_Interrupt problem

Posted on September 03, 2017 at 10:27Hello sir,HELLO EVERYBODY,I have a question about LIS3MDL.   Expecially, interrupt problem.I am using LIS3MDL below sequence.=================================================================================1. In ...

LIS2DH FIFO in SPI mode

Posted on July 13, 2017 at 14:06I did not quite understand from the pdf when reading 32*3 samples from the FIFO in SPI mode, can I set the SPI starting address at OUT_X_L (28h) with the SPI's MS bit raised and then read in a constant SPI read stream...