MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LPS22DF I3C addressing

Dear forum,We plan to assemble five LPS22DF sensors on the same I3C bus and (off course) to address them individually. According to the datasheet (7.4.1 MIPI I3CSM CCC supported commands) the answer to GETPID can only have two values, depending on SD...

tcachat by Associate II
  • 971 Views
  • 1 replies
  • 0 kudos

LIS3MDL not responding over SPI on custom PCB

Hi,I'm designing a flight controller pcb using several ST mems sensors, (LSM6DSO, LIS3MDL, LPS22HH) and interfacing them to an STM32H743IIT6 microcontroller over a shared SPI bus. I'm on the second iteration of this board, all sensors worked on the f...

VictorK_7-1725716130081.bmp VictorK_8-1725716140311.bmp VictorK_6-1725714206425.png VictorK_2-1725713533727.png
VictorK by Associate
  • 1085 Views
  • 2 replies
  • 2 kudos

Resolved! LIS2DE12 Tolerance

I am using a LIS2DE12 to detect when a mechanical shock occurs to my device. The datasheet provides only nominal values for the sample rate and the sensitivity.What is the tolerance on the sample frequency, I am using the ODR nominal rate of 5376 Hz?...

Resolved! How to select I2C on STEVAL-MKI109V

Hi All I am running Unicon GUI on Windows 10 and using it to communicate with STHS34PF80 sensor plugged onto STEVAL-MKI109V dev board.I can fully interact with the senor via the GUI app. Meaning reading and writing all registers of interest.I however...

ola by Associate III
  • 1012 Views
  • 4 replies
  • 0 kudos