MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MotionSP FFT q15 or q31 instead of float32

Hello Community,I am trying to implement a basic FFT computation on our STM32G0 MCUs using MotionSP for a 16-bit accelerometer signal.I am not sure why does MotionSP by default uses float32 for FFT when the original sensor signal is 16-bit?Can I then...

Chubs by Senior
  • 590 Views
  • 1 replies
  • 0 kudos

Resolved! LPS22 sensor

Hello,I'm trying to disable temperature compensation on the lps22hh sensor, does anyone know if there's a specific register i can manipulate? Thanks!

ILPS28QSW Gel Info

Hello all,I am looking for more info on the gel used with ILPS28QSW.We want to use it in an application where the sensor may be submerged in 10% to 40% alcohol v/v for extended periods of time. Will the sensor be okay? Or is there another product whi...

Resolved! IIS3DHHC Sensitivity

Regarding the sensitivity of IIS3DHHC, the datasheet says 0.076mg/digit. It is written. To be exact 5g/2^16 (= 0.07629mg/digit) Is that correct?Thanks!

totaw.1 by Associate II
  • 736 Views
  • 2 replies
  • 0 kudos

STHS34PF80 Sensor's Power Consumption is very high.

Hello there, I am currently working on a project where I am prototyping STM32WL55 with an STHS34PF80 sensor to detect the presence. The presence detection is excellent and robust so far. However, the power consumption seems to be very high at the mom...