MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Over-molding of LSM9DS1

Posted on March 22, 2018 at 08:57Hi, This question is regarding the e-packaging of the LSM9DS1 sensor PCBA Instead of packaging it in the plastic casing, We are planning to cover the PCBA with the overmolding material to cover the whole PCB includin...

LIS2DH12: High and Low Interrupt for all axis

Posted on April 02, 2018 at 21:52I'm currently trying to configure the LIS2DH12 sensor to enable high and low interrupt on all axis.My target is to implement a shock detection and therefore I plan to use all axis (x,y,z) and as well high and low thr...

Philipp D by Associate II
  • 3094 Views
  • 5 replies
  • 0 kudos

LIS3DH low output registers outputting random data

Posted on March 30, 2018 at 18:51I have the LIS3DH accelerometer set for no FIFO, X,Y & Z output, Hi Res. I have BDU turned on.I am reading the high byte of each axis and getting the expected data which changes with accelerometer position. In all ca...

gbarbour by Associate III
  • 1126 Views
  • 2 replies
  • 0 kudos

lsm6dsl_reg.h possible error ?

Posted on April 01, 2018 at 17:28Hi, When using lsm6dsl_reg driver files I've stumbled on the following angular velocity conversion macros.The math seems wrong... Can ST verify this?Thanks#lsm6dsl_reg

LSM303DLHCTR - Peak Current Consumption Issue

Posted on April 02, 2018 at 19:18I'm using an LSM303DLHCTR in an application where I'm reading its X, Y and Z magnetometer values once per 20 ms, and have noticed that the chip seems to consume 10 mA or more of current from its 3.3V supply (VDD pin)...

HTS221 Cal. Coeficients

Posted on March 27, 2018 at 09:03Hello,I implemented the software for the HTS221 in my project and all is working. But what I find strange is this, some calibration coefficients are negative!H0_T0_OUT is -2H1_T0_OUT = -11728Although they are negativ...

LSM6DS3 Data ready Interrupt

Posted on March 27, 2018 at 09:13Hi, I`m facing a problem to get data ready interrupt on INT1.Use I2C communication.Trying to make fifo work and stuck with that, so started from data ready. According to Application notes :1 Write CTRL9_XL = 38h // A...

0690X00000604SiQAI.jpg

Voltage drop when connecting IKS01A2 to B-L072Z-LRWAN1

Posted on April 03, 2018 at 18:10So the B-L072Z-LRWAN1 board is configured to be powered through the 3.3V pin by removing SB6 and R26. Furthermore, the ST-LINK was disconnected by removing SB28, SB29 and SB37. When testing with some example code and...

How does LIS3DH configure automatic sleep and arousal?

Posted on March 16, 2018 at 11:40 I want to be able to when the device has detected movement, LIS3DH to wake up from sleep mode, and at a higher rate to detect more than I get a set of threshold, then the interrupt, to remind me of the MCU. I trie...

? ?_3 by Associate II
  • 3903 Views
  • 9 replies
  • 0 kudos