cancel
Showing results for 
Search instead for 
Did you mean: 

Voltage drop when connecting IKS01A2 to B-L072Z-LRWAN1

Robbe Elsas
Associate
Posted on April 03, 2018 at 18:10

So the B-L072Z-LRWAN1 board is configured to be powered through the 3.3V pin by removing SB6 and R26. Furthermore, the ST-LINK was disconnected by removing SB28, SB29 and SB37. When testing with some example code and the X-NUCLEO-LPM01A power board everything works fine. However, when connecting the IKS01A MEMS shield to the B-L072Z-LRWAN1 board, either with the arduino connector or with the dedicated J2 header, the system voltage drops from 3V to approximately 1.4V causing the B-L072Z-LRWAN1 to halt correct operation. I haven't made any chaanges to the default solder bridge/jumper config of the IKS01A2 MEMS shield and its datasheet is wildly obscure when it comes to the power config. Has anyone had a similar problem and if so how do I fix this?

#b-l072z-lrwan1 #iks01a2
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0