MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Questions about the interrupt config for Lis3dx

Posted on April 08, 2018 at 08:261) CTRL_REG3 (22h)Can I set both I1_IA1 and I1_IA2? 2) What is I1_321DA? 3) Our project uses two threshold, one for stronger force (e.g. collision), the other for weaker force (e.g. impact). I assume I should set INT...

0690X0000060ASxQAM.png 0690X0000060APaQAM.png 0690X0000060ATHQA2.png
Kefei Yao by Associate III
  • 1977 Views
  • 3 replies
  • 1 kudos

Resolved! Can't get IG2 work on either INT1 or INT2 for Lis3de

Posted on April 08, 2018 at 13:13I encountered a problem that IG2 doesn't get detected on either INT1 or INT2 pin. I confirm the IG1 work on both INT1 and INT2. Followings are the combinations I tried (CTRL REG1,2,4,5 kept unchanged):The INTx_CFG,IN...

Kefei Yao by Associate III
  • 1145 Views
  • 1 replies
  • 0 kudos

AIS1120SX

Posted on April 08, 2018 at 18:01Has anyone developed STM32 code for the AIS1120SX accelerometer?-Bruce#accelerometer-ais1120sx*

Resolved! LIS3DH outputting unexpected data

Posted on October 16, 2017 at 14:15Hello,I am trying to log accelerations above 2g. To do so I parametrized the LIS3DH as following:- CTRL_REG0: 0x10- CTRL_REG1: 0x57 (100Hz + Xen + Yen + Zen)- CTRL_REG2: 0x00- CTRL_REG3: 0x40 (IA1 on INT1)- CTRL_RE...

LSM303AGR - Magnetometer: Perpendicular Readings

Posted on April 02, 2018 at 21:07Hi!I had a previous post asking how to interpret the values being drawn from the chips registers and I was able to get that working. (https://community.st.com/0D50X00009XkWYOSA3 )However, it only works as a 360 degre...

0690X0000060ANTQA2.png

HTS221 accuracy and TN1218 question

Posted on May 06, 2017 at 22:23Hello,I'd like to ask you about opinion on accuracy of HTS221 sensors, both factory mounted on X-NUCLEO-IKS01A1 boards (powered by Nucleo board @ 3.3 V).I get quite surprising results from these sensors, compared to re...

Resolved! LSM303AGR self test always fails

Posted on March 29, 2018 at 23:41Hello, I'm using an LSM303AGR thru I2C, and after a little struggling, everythings looks fine. I can read any of the 6 axes with what seems to be the right values, and the read values react correctly when I tild my b...