MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DE12 WTM signal not cleared when reading from FIFO

Posted on April 17, 2018 at 23:55Hi All,I'm using an LIS2DE12 in stream mode with the watermark set to 15 FIFO entries and with the WTM bit being driven out INT1. When INT1/WTM goes high, I read out 16 FIFO entries and, as expected, INT1/WTM goes lo...

LSM9DS1 standby consumption

Posted on April 11, 2018 at 17:33What is LSM9DS1 standby consumption (all sensors off)?The datasheet says nothing, no value in Electrical characteristics section.Its predecessor LSM9DS0 has 6uA typical.

LSM6DS3 & m24c64 power consumption high

Posted on February 01, 2018 at 16:17Hello All,We are doing a wearable product where we using LSM6DS3 & M24C64 but power consumption much high than specified.LSM6DS3 is taking around 300uA just by powering on. As we understand from datasheet by defau...

piyush by Associate
  • 1543 Views
  • 2 replies
  • 0 kudos

LIS3DH - Motion and crash detection

Posted on February 26, 2018 at 12:02Hello allMy goal is to use two INT pins to generate two interrupts in a device which will be used in a car. INT2 will be pulled when a crash of the car is detected and INT1 when the car moves.Here is my init setti...

Resolved! LIS3DH and LSM9DS1 accelerometer comparison

Posted on April 13, 2018 at 14:16Hello,I am trying to compare LIS3DH and LSM9DS1 (accelerometer part) and I am suprised by the result:The LIS3DH has the configuration: CTRL1: 0x67 (ODR = 200Hz, LPen=0, ) CTRL4: 0xA8 (BDU, 8g, HR)   => sampling frequ...

0690X00000604aSQAQ.jpg
Mich1 by Associate III
  • 1314 Views
  • 2 replies
  • 0 kudos

LISD2E12 INT1_THS not changing tilt threshold

Posted on February 23, 2018 at 21:28 The INT1_THS register value does not seem to change the threshold at which an event is triggered. I can read and write the INT1_THS(0x32) so I know my writes are working. I poll the INT1_SRC register and watch t...

LSM9DS1 and LSM6DS3 accelerometer resolution

Posted on December 01, 2015 at 22:29HiIm having some trouble confirming whether the resolution from the accelerometer in the LSM9DS1 and also LSM6DS3 is actually 16 bits ?The datasheet for both sensors say the output resolution is indeed 16 bits, bu...

andres by Associate
  • 1715 Views
  • 2 replies
  • 0 kudos

See anything wrong with bit bang driver for HTS221??

Posted on April 03, 2018 at 04:41I am writing a bit banging SPI driver for the HTS221 with no success,I drive the SDO data just before the falling clk endand I read the SDI data on the rising clk edge. I have included a screen capture of the Saleae ...

LSM303C magnetometer interrupt capabilities

Posted on April 12, 2018 at 10:46Dear all,referring to the LSM303C data sheet, I'd like to know what exactly is to be understood with 'The system can generate an interrupt signal for ... magnetic field detection'.I am interested in an application wh...