Question
OTA for SensorTile
Posted on September 26, 2017 at 22:07
I am using the code from STM32CubeFunctionPack_MOTENV1_V3.0.0 for sensor tile.
Initial I used the STlink to load the 'Projects\Multi\Applications\MOTENV1\Binary\STM32L476RG-SensorTile' MOTENV1_ST_BL.hex.
Then connect to the ST BlueMS.
When I trying out the 'Firmware upgrade' OTA feature in the Apps.
I select the 'MOTENV1_ST.bin' and copy it to the Phone.
Tried a few times of the OTA procedure and it always fail at the end 'Error sending the data'.
Is the binary file used on Phone for OTA correct ??
Regards,
Felix