Skip to main content
Francesco Murru
Associate
September 21, 2017
Solved

LIS2DH incorrect I2C address?

  • September 21, 2017
  • 2 replies
  • 1798 views
Posted on September 21, 2017 at 23:49

Hi all,

today I started a new project using the LIS2DH accelerometer (I2C mode). Previously I already used, very successfully, LIS3DH, always in I2C mode. Seeing the datasheets, in the basic functionatity, LIS2DH and LIS3DH are pratically the same object (the LIS3DH has just 3 extra ADC channels...): same registers, same setup and, theorically, same I2C Address, (0x18 when SA0 = 0, 0x19 when SA0 = 1). So, I was expect an easy porting of my code because, I repeat, theorically, LIS2DH and LIS3DH, are the same device. Theorically!

I don't know why, but using 0x18 (my SA0 is 0) the LIS2DH do not comunicates.

I was going crazy: I do three times a rework of the pcb (I was thinking that maybe the problem was the board): nothing, nothing and nothing.

So I had this idea: I checked all I2C's space address, from 0x00 to 0x7F. I got no response, as previously, at 0x18 but, incredible, I got a response at 0x29.

Mmmm...very strange but...Ok, I updated my .c library using this new address and...WOW, LIS2DH works!

But I still have a doubt: how is this possible??

The datasheet of LIS2DH no reports any errata about the I2C address...

Any idea?

Regards,

Francesco

NOTE: the I2C bus is shared whit a MS5803 barometric sensor, that correctly works with his address (0x77)

    This topic has been closed for replies.
    Best answer by Miroslav BATEK
    Posted on September 22, 2017 at 09:52

    Are you sure it is LIS2DH? It would be possible that someone mix up the LIS2DH with LIS2DE which has the I2C address 0x28/0x29.

    But in this case the SA0 should be 1 to set the address to 0x29.

    May I know, where did you buy the part?

    2 replies

    Miroslav BATEKBest answer
    ST Employee
    September 22, 2017
    Posted on September 22, 2017 at 09:52

    Are you sure it is LIS2DH? It would be possible that someone mix up the LIS2DH with LIS2DE which has the I2C address 0x28/0x29.

    But in this case the SA0 should be 1 to set the address to 0x29.

    May I know, where did you buy the part?

    Francesco Murru
    Associate
    September 22, 2017
    Posted on September 22, 2017 at 10:33

    OPS! 

    A colleague has done the purchase for me, and yes, It has buy a LIS2DE!! Doh! His fault made me a fool!

    :(

     

    :(

    Thank you Miroslav, you solved the mystery!