MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DH12 proper free-fall detection settings

Hi,I'm having trouble following how to properly setup free fall detection on the LIS2DH12. I'd like to generate an interrupt when the device goes from rest to free falling for a couple feet. The duration of the fall would be approximately 200ms. I'm ...

Resolved! MotionFX VS MotionDI lib for 6axes fusion

Hello,both of MotionFX 6X and MotionDI return the same output (rotation vector, quaternion, gravity, and linear acceleration)so what is the difference between theme, and witch one is more suitable for 6 axes fusion ?should i implement additional cali...

malarab by Senior II
  • 593 Views
  • 1 replies
  • 0 kudos

LSM6DSL step counter

we are using this LSM6DSL sensor for our smart ring device. and we also implement step counter which is inside of this IC to calculate step for user, while he wears the smart ring on his finger.I'd like to know if there is any performance difference ...

sangyun by Associate
  • 444 Views
  • 1 replies
  • 1 kudos

LSM6DSO Register - WAKE_UP_THS - 0x5B

Hi,  I am looking at the LSM6DSO device, and I am unclear what the "USR_OFF_ON_WU" bit does in the "WAKE_UP_THS " register. Does this bit: Drive the Wake-Up function with offset corrected accelerometer data? 0 means not offset corrected, 1 means offs...

Dude by Associate III
  • 587 Views
  • 1 replies
  • 0 kudos

LSM6DSO - WAKE_UP_THS - WK_THS

Hi,    I'm looking through the LSM6DSO32X datasheet, and I'm having a hard time finding out information about certain register data bits. For instance, register "WAKE_UP_THS" (0x5b) has 6 bits labelled "WK_THS[5:0]". Are these bit signed or unsigned?...

Dude by Associate III
  • 632 Views
  • 1 replies
  • 0 kudos

ASM330LHB performance data

My team is looking at what performance data ST has on file for the ASM330LHB. Specifically ​random walk and bias stability performance of accelerometers and gyros over the entire operating temperature range (-40C to 105C).

hmiller by Associate
  • 660 Views
  • 3 replies
  • 0 kudos

Resolved! empty SD card sensor tile probox

good morning. i am actually trying to load on my an sd card my data of the sensor tile.box. Unfortunately, I only get blank tables with only the top written. I uploaded a configuration to make it and then uploaded as seen on those photos. am I missin...

Jad_0-1726993052664.png Jad_1-1726993077075.png Jad_2-1726993122799.png
Jad by Senior
  • 719 Views
  • 1 replies
  • 0 kudos