MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2HH12TR Tap Detection Firmware Example

Posted on April 03, 2017 at 01:10I have LIS2HH12TR on a PCB. I want to implement Tap Detection. I could not find a direct Register for configuring Interrupt for a tap. It would be great to refer to Example code for Tap Detection using Raw Accelerome...

V2.2.0 BlueMicrosystem2 would not build SW4STM32

Posted on May 05, 2017 at 21:45I just started the SensorTile project and have installed the AC6 System Workbench.Download 2 different SDK from ST.STLKT_v1.2.0BlueMicrosystem2_V2.2.0The STLKT is fined, I could build and load the sample code into Sens...

lis2dw12 sensor SPI CPHA and CPOL setting

Hi all,I'm using lis2dw12 sensor and interfaced with SPI. In which SPI mode i can get proper data from the sensor?CPHA = 0, CPOL = 0;CPHA = 0, CPOL = 1;CPHA = 1, CPOL = 0;CPHA = 1, CPOL = 1;Thanks and regards,Basavanagouda

VL53L1X readings unreliable when no object in front

I am testing the VL53L1X in medium measurement mode at 200ms timing budget I get 140cm weak return signal value even when there is no object in front.In long measurement mode with 300ms timing budget with no object infront the values I get are jitter...

AKhan.15 by Associate II
  • 813 Views
  • 0 replies
  • 0 kudos

LSM303C Accelerometer Activity/Inactivity Interrupt

Hi,This question was asked by someone 4 years ago and hasn't been answered yet. Hope it gets answered this time around.I have been trying to experiment with the interrupt functionality of LSM303C with no success.So far I have followed all the steps i...

SLokh by Associate
  • 743 Views
  • 0 replies
  • 1 kudos

Do the LIS3MDL Reserved Pins need to be connected?

Hi, we have a board with several I2C based sensors on it, including the LIS3MDL and LIS3DH.The 3DH works like a treat, but I cant get any communication from the 3MDL. The only thing I can see that would cause this is a discrepancy with our board desi...

JRule by Associate
  • 1780 Views
  • 6 replies
  • 0 kudos