Skip to main content
Dilbert K
Associate III
May 5, 2017
Question

V2.2.0 BlueMicrosystem2 would not build SW4STM32

  • May 5, 2017
  • 5 replies
  • 1126 views
Posted on May 05, 2017 at 21:45

I just started the SensorTile project and have installed the AC6 System Workbench.

Download 2 different SDK from ST.

STLKT_v1.2.0

BlueMicrosystem2_V2.2.0

The STLKT is fined, I could build and load the sample code into SensorTile without issue.

  • BlueMicrosystem2_V2.2.0\Projects\Multi\Applications\BlueMicrosystem2\SW4STM32\STM32L476RG-SensorTile\STM32L4xx-SensorTile

AC6 System Workbench

But when trying to build above project under '

BlueMicrosystem2_V2.2.0

', the build failed... with basic missing define

Symbol 'BNRG_SPI_EXTI_PIN' could not be resolved main.c /STM32L4xx-SensorTile/BlueMicrosystem2/User line 2036 

Symbol 'NULL' could not be resolved bluenrg_gap_aci.c /STM32L4xx-SensorTile/Middlewares/STM32_BlueNRG/HCI/Controller line 1312 Semantic Error

I tried to build the project using IAR, it passed without issue... but I don't have full license... Have to use AC6 with Eclipse.

Anyone has ideas what path configure is required ?

    This topic has been closed for replies.

    5 replies

    Dilbert K
    Dilbert KAuthor
    Associate III
    May 5, 2017
    Posted on May 05, 2017 at 21:55

    Seems to be a installation setup (Path issues)....

    1.  Using the Stand alone AC6 System Workbench --> OK
    2. Using Eclipse with AC6 installed as software --> ERROR

    However, both are OK for projects under 

    STLKT_v1.2.0\Projects\SensorTile\Applications

    Dilbert K
    Dilbert KAuthor
    Associate III
    May 19, 2017
    Posted on May 19, 2017 at 21:03

    Issue due to#elif STM32_SENSORTILE

    https://community.st.com/0D50X00009XkY02SAF

    sener
    Visitor II
    December 18, 2018

    Hi,

    I am having the same issue. Have you already solved the issue, if so how?

    Note that: The link you provided is not exist anymore.

    Thank you.

    sener
    Visitor II
    December 18, 2018

    I guess that I have found the missing piece. At least it worked for me.

    For the records,

    When I added the line below, no error anymore (although the warnings are still there)

    #include "SensorTile_BlueNRG.h"

    Dilbert K
    Dilbert KAuthor
    Associate III
    January 2, 2019

    Go to project -> Properties -> MCU GCC Compiler -> Preprocessor

    Change the define to follow (add =1) from original code

    STM32_SENSORTILE=1