Hello, below the setting we use. Note the system behaves as expected if the RFID field is off.register Register name value bit setting0x20 Ctrl 1 0x57 datarate 100hz, Low power enable off, all axis enabled0x21...
The RFID is at 13.56MHz. What we have done so far is to test the accelerometer on the PCB with and without the RFID active. When we saw that the chip showed undesired behavior with the RFID active, we tried relocating it. This was done by removing th...