MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Basic Functioning and UNICO

HiI am new to this lsm6dsoi am currently using STEVAL-MKI109V3 with STEVAL-MKI191V1 using unico.What i a getting is that "ADAPTER BOARD NOT SUPPORTED" I has also tried Serial Terminal still getting same result with *setdb191v1any help with this?

VBans.16 by Associate II
  • 1040 Views
  • 1 replies
  • 0 kudos

Problem with LIS3DH thresholds

Posted on September 02, 2017 at 13:08Hello allI have a problem with setting LIS3DH module to detect movement.To be more precise, I want the device to set the INT1 pin down when the it experiences 32mg acceleration change for 0.5 second. Here are my ...

Where to find the documentation of the VL53L1X registers?

Hi everyone, I do not post very often to ask for support but this time I really need help :smiling_face_with_halo: I am working with the VL53L1X (more precisely the Breakout boards which are really great). I successfully managed to get a distance val...

Error while Integrating Acceleration to get Position after Fusion

Hello,I need to get position and track the motion of the IMU from the acceleration and other data it gives. I am using a Nucleo STM32F401RE board and a X-Nucleo- IKS01A2 MEMS sensor. I am using the DataLogFusion example in Unicleo-GUI. To get positio...

engtec by Associate
  • 1420 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DS3 absolute maximum acceleration

Dear All,I have several questions regarding the absolute maximum acceleration, which the chip (LSM6DS3) can resist. The Datasheet says it is 10000g for 0.2 msMy questions are:* Is there any difference if the chip is powered or unpowered?* What does t...

SGats by Associate
  • 1463 Views
  • 2 replies
  • 0 kudos

CubeMX + NUCLEO-L053R8 + X-CUBE-MEMS1 can't be built

Using CubeMX v5.0 and FW_L0_v1.11.0 I'm generating new project from scratch.Project has initialized (using HAL) UART2, I2C1 (on alternate pins PB8, PB9), GPIOs, EXTIs and clock. UART2, I2C1 and EXTI interrupts are enabled and IRQ handlers generated b...