MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12 Orientation (Tilt) implementation

I have followed the DT097 (design tip for 6d orientation detection). When I moved from vertical position (face up) and rotated the board around X (or Y) axis the interrupt that I got ia when it is angle-complement of what I have selected e.g. 20 de...

erush by Associate II
  • 3562 Views
  • 8 replies
  • 0 kudos

STEVAL-MKI109V3 not responding post firmware update.

The device wasn't being recognized or accepted on the Unico software, and on the basis of something I read on the forums, I decided to update its firmware. I used the Dfuse program, and was told that updating the firmware was successful. However, whe...

MRanj by Associate
  • 1781 Views
  • 3 replies
  • 0 kudos

BlueCoin demo for beamforming not working.

Hi, i'm trying to run the beamforming demo on bluecoin. connected the bluecoin core to coin station and then connected to laptop. It has been detected on port and I recorded voice on audacity by choosing stm mic. The issues is no matter I rotate the ...

VPotl by Associate II
  • 1507 Views
  • 2 replies
  • 0 kudos

Problems with saving PDM audio to SD card

Posted on April 01, 2018 at 20:13I am trying to modify the SensorTile AudioLoop sample project to save the audio to an SD card, instead of sending it out to the audio DAC and USB. I have successfully managed to save some audio data to the SD card, b...

Norman S by Associate II
  • 3731 Views
  • 5 replies
  • 0 kudos

Problems with MISO signal with SX1276

Hi,I'm new to the forum here so please be kind if anything is not getting too clear or any information is missing.Is was trying to prgramm a SX1276 using CubeMX. So the programm seems to work and I can see signals in 'Logic'. I can see the clock and ...

0690X000006D8bbQAC.png 0690X000006D8bWQAS.png
BTiet by Associate
  • 756 Views
  • 0 replies
  • 0 kudos

barometer membrane reference?

Hello,LPS22HH hardware guidelines talks about a membrane to protect from rain or dust. Do you have some references of such membranes please?Best regardsMich

Mich1 by Associate III
  • 1118 Views
  • 1 replies
  • 1 kudos

ST LIS2DE12 WHO_AM_I?

Dear ST Community Members,I tried to understand...page 25 ST LISDE12.pdf..................Data are transmitted in byte format (DATA). Each data transfer contains 8 bits. The numberof bytes transferred per transfer is unlimited. Data is transferred wi...