MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ellipsoid fitting for magnetic values (LSM303AGR)

Hello everyone,I started with the implementation of the rotated ellipsoid fitting described in DT0059 for the LSM303AGR compass. There is as well a sample matlab code which I use to verify my implementation. My software inside the microcontroller cal...

0690X000006C2P4QAK.png
DZimm.16 by Associate
  • 487 Views
  • 0 replies
  • 0 kudos

SensorTile temperature readings

Posted on July 07, 2018 at 14:09I am attempting to use a SensorTile for continuous audio recording and environmental monitoring, recording data to the SD card hosted in the cradle.  I am finding that temperature readings are unreliable/unusable, whi...

LSM9DS1 Magnetometer readings make no sense?

Hello!I am working with the LSM9DS1 and am having trouble with my magnetometer.I tried following Application Notes in which pitch, yaw and roll are calculated but had no success. I tried tracking down the error and I found the following problem: My m...

RReic by Associate
  • 730 Views
  • 1 replies
  • 0 kudos

In HTS221 sensor not getting correct Humidity data

Posted on September 22, 2015 at 08:14I am using HTS221 , and I am taking value from HTS221 via I2C.Here i was successful to get correct temperature data you can see in attach .txt file.But for Humidity i am getting values but they are not as per env...

jayesh1 by Associate
  • 1801 Views
  • 5 replies
  • 0 kudos

Begining with LIS3DHTR Sensor for tap detection

Require some basic knowledge to use LIS3DHTR https://store.ncd.io/product/lis3dhtr-3-axis-accelerometer-digital-output-motion-sensor-i2c-mini-module/ to work with arduino and make the TAP detection solution but to make it work. As beginner in this, I...

Resolved! LIS2HH12 - Meaning of RES pin

Hello,I have a board on my desk where the RES pin (#5) of LIS2HH12 is not connected.The data sheet says, Connect to GND. OK ... not good ...As I do not get any response of the accelerometer via I2C, I would like to know if this pin is the reason. I c...

s m by Associate III
  • 1319 Views
  • 3 replies
  • 0 kudos

Failure reading from LIS3DSH SPI interface

I am interfacing a LIS3DSH using SPI. My MCU is a Texas Instruments MSP432.When writing and checking configuration registers, even-addressed ones do not return the expected value.After sending a byte, MSP432 MOSI retains the value of its MSB. This is...

0690X000006C44SQAS.png 0690X000006C3yoQAC.png 0690X000006C3z8QAC.png 0690X000006C3zSQAS.png
GioP by Associate II
  • 639 Views
  • 0 replies
  • 0 kudos

MEMS measurement ranges hardware details

Hello everyone,How does MEMS measurement ranges realized in hardware in details? Does it use: 1. Amplifiers with different gain ratios? 2. ADC with as many bits as need to serve maximal range with minimal resolution? 3. Does different MEMS cells used...

LIS3MDL Magnetometer data reading Error

Hi All,I am working on the LIS3MDL register on my board. But When I try to measure the Magnetic field Produced by motors, I am getting very high deviation.My settings for the LIS3MDL are as below.0x22 -- 0x00 (also tried with 0x22 -- 0x03)0x21 -- 0x0...

HGohe by Associate II
  • 2256 Views
  • 8 replies
  • 0 kudos

STMPE610 - cant read data

im using the feather nrf52832 with the featherwing.i can read the ID by sending 0x00 as [0x80,0x81,0x00] = getting 0x0811i tried to do the same with TSC_DATA_X 0x4D , but i can read any data from the sensor.my init is :  writeRegister8(SYS_CTRL2, 0x...

ykein by Associate
  • 607 Views
  • 0 replies
  • 0 kudos