cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2HH12 - Meaning of RES pin

s m
Associate III

Hello,

I have a board on my desk where the RES pin (#5) of LIS2HH12 is not connected.

The data sheet says, Connect to GND.

OK ... not good ...

As I do not get any response of the accelerometer via I2C, I would like to know if this pin is the reason. I can't easily connect it due to the package ...

Does RES stand for RESET or does anyone from ST can confirm that connecting RES not to ground results in having no I2C access?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee

I can confirm that LIS2HH12 can work even if the RES (5) pin is unconnected, bun in this case the noise of the accelerometer can increase.

View solution in original post

3 REPLIES 3
Miroslav BATEK
ST Employee

I will check with the product specialist, but I doubt unconnected RES pin is the reason why your device doesn't work. I would keep looking for another reason.

The RES means RESERVED and is not needed for sensor operation, but should be polarized.

Miroslav BATEK
ST Employee

I can confirm that LIS2HH12 can work even if the RES (5) pin is unconnected, bun in this case the noise of the accelerometer can increase.

s m
Associate III

Thanks, I desoldered it and I figured out that it was not soldered correctly.