MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMPE610 - cant read data

im using the feather nrf52832 with the featherwing.i can read the ID by sending 0x00 as [0x80,0x81,0x00] = getting 0x0811i tried to do the same with TSC_DATA_X 0x4D , but i can read any data from the sensor.my init is :  writeRegister8(SYS_CTRL2, 0x...

ykein by Associate
  • 607 Views
  • 0 replies
  • 0 kudos

VL53L1x factory default ?

Since there's no information on the registers in the datasheet, and half of the API is in the documentation. I'd like to know if there's a reset/factory default settings for the chip ?I was building the platform file and sent a lot of crap to the dev...

SBeno by Associate
  • 536 Views
  • 0 replies
  • 0 kudos

Would like to receive audio stream from Sensor Tile board

Hello,I have STEVAL-STLKT01V1 sensortile board and would like to stream the audio from sensortile board to raspberry pi board via BLE interface.https://www.st.com/en/evaluation-tools/steval-stlkt01v1.htmlFor this, ST provided BlueVoice python framewo...

IIS2DH axis Z not working

Hello everyone,I have an issue with the IIS2DH accelerometer when I try to pool data from it.My setup is: STM32L442 connected to the IIS2DH using SPI interface and sending data through USART to Tera Term (using a FTDI cable).First I have a small init...

when i connect the x-nucleo-iks01a2 board to the p-nucleo-lrwan1 dev kit i get PHY txtimeout error even do the frist payload does reach the application but no others do.

Hi, I am following manuals UM2084 and UM2073 and with out the iks01a2 board everything thing works fine with the ***** payload reaching the application over the web every-time, but when i reset up and add the iks01a2 board to the dev kit i get PHY tx...

LSM6DSL Fifo Data Set Corrupted

Hello,I am using the LSM6DSL in FIFO Continuous Mode. Fifo ODR is equal to the Accelerometer and Gyroscope ODRs (no decimation configured). Data are retrieved from fifo after the FIFO_FULL interrupt is triggered.  I have a problem that appears after ...

OEl F by Associate
  • 905 Views
  • 1 replies
  • 0 kudos