MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HTS221 sensor driver

In CubeMX the HTS221 driver was chosen.While looking to use the sensor within the code, i can't find any documentation how to initialize the sensor.In the HTS221 headerfile i can find: HTS221_Init(HTS221_Object_t *pObj)This function uses a HTS221_Obj...

0690X0000087ocpQAA.png 0690X0000087ofKQAQ.png

LIS2DE12 Event Max Values.

Dear support,I'm looking for an accelerometer and the one we work with is normally LIS2DE12, but I think it does not work for the product I'm looking for.In the INT1_SCR register, high and low interruption events can be enabled in the different axes,...

JForm by Associate II
  • 3689 Views
  • 6 replies
  • 0 kudos

LPS22HB coated by moisture-proof coating

When we applied moisture-proof coating to the substrate, we also coated the LPS22HB.In this case, does the coating affect the measurement?If so, is it okay to rub the sensing area to remove the coating?

KIwan by Associate
  • 1047 Views
  • 1 replies
  • 0 kudos

LIS3DH temperature sensor interpretation

Is the accelerometer temperature output in OUT_ADC3 still 8 bits if the LPen bit in CTRL_REG1 is cleared?If that is the case, does the temperature change with one digit in OUT_ADC3_H per °C?

MLund by Associate
  • 1220 Views
  • 1 replies
  • 0 kudos

ISM330DLC data rate for higher precision

We understood the ODR and correlated filtering. A following micro-controller application performs further filtering with averaging values to 10 per second. Aimed is calculating an angle derived from the rotational speed. Precision should be about or ...

pl by Associate II
  • 1125 Views
  • 1 replies
  • 0 kudos

LSM6DSL fifo-mode power consumption issue.

Hi!We configured it fifo contineous mode to further reduce the current consumption of the lsm6dsl mounted on our own board with nRF52832(nordic semiconductor), but rather the current consumption has increased. Total current consumption has increased ...

jcho.8 by Associate
  • 878 Views
  • 0 replies
  • 0 kudos

How to use MKI197V1 by MKI109V3 ?

Hi,I have a MKI109V3 and one MKI197V1.I have downloaded the related tools&software of MKI109V3 then I opened the DfuSe Demo from en.stsw-mki109w / MEMS_Demonstration_Kit_SW_package_v8_0_WINDOWS and upgraded ProfiMEMSToolV2.40.1.dfu from ProfiMEMSTool...

spark by Associate II
  • 1045 Views
  • 0 replies
  • 0 kudos