How to enable an interrupt on LIS3DH that detects twisting of the wrist.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-03-19 3:24 AM
I have enabled 2 interrupts on the LIS3DH all on the I2C Bus :
1) Data Ready Interrupt
2) Orientation Change Interrupt
But during runtime only the Data Ready Interrupt is working. While reading the INT1_SRC register no value is generated. Even after disabling Data Ready Interrupt, I am unable to access the Orientation Change Interrupt.
I have configured the following registers on the LIS3DH
CTRL_REG1(0x20) Value(0x57)
CTRL_REG3(0x22) Value(0x00)
CTRL_REG6(0x25) Value(0x02)
INT1_CFG(0x30) Value(0xE5)
INT1_THS(0x32) Value(0x07)
I have been trying to read the interrupt coming from INT1_SRC(0x31) in the in_pin_handler function and it always returns 0x00
- Labels:
-
Accelerometers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-03-19 5:00 AM
hi, do you drive the data-ready interrupt (ZYXDA bit) on INT1?
If you want to route the Orientation Change interrupt on INT1 pad please change --> CTRL_REG3(0x22) Value(0x40)
Btw, please try also to change the INT1_DURATION to 01h for check