MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH, how to calculate the x, y, z ?

Hi team,I am working on LIS3DH sensor, and found a lot resource from internet.​But I go confused when I saw difference formula to calculate the OUTPUT_X or OUTPUT_Y.​Source1:dt_usr[0] = float(short((data[1] << 8) | data[0]) >> 4) * fs_factor;https://...

JChen.16 by Associate
  • 1397 Views
  • 1 replies
  • 0 kudos

Sampling data at 1 KHz with LSM6DSM

Hello,I am using LSM6DSM in Mode 1, 250 dps full scale, high performance mode enable and I am reading data from OUTZ_L_G and OUTZ_H_G registers. My application must sample gyro data at 1 KHz, how have I to configure ODR, FTYPE, etc to get data in the...

steba by Associate
  • 1013 Views
  • 1 replies
  • 0 kudos

LIS3DH wrong address?

Hi,I got some LIS3DH that are not responding to 0x19 neither 0x18... When I run a I2C sniffer, it finds a device on 0x09...Just wondering if someone can confirm the attached component is a LIS3DH?Thanks

0690X0000088mfAQAQ.jpg
lsb by Associate
  • 1154 Views
  • 2 replies
  • 0 kudos

STEVAL-SMARTAG humidity sensor readout problem

I have flashed the example code from the function pack on 2 STEVAL-SMARTAG modules using a Nucleo STLink. After flashing, I get very different (incorrect) values from the humidity sensor (31% whereas the original sensor, as purchased, read the corre...

Peter S. by Associate II
  • 1621 Views
  • 3 replies
  • 0 kudos

Design issue of VL53L0X

Hello,I am impressed by this tiny but effective sensor module. In fact, I am trying to design lidar system using VL5310X. The thing is that, I want to integrate my fabricated laser and photodiode with this module. Therefore, is there any other produc...

MPark.7 by Associate
  • 685 Views
  • 0 replies
  • 0 kudos

How to calibration fomula of CT for STPM34 ?

Hi All; I would like to calculate CT. I have formula below. I factor = VREF / (AI * CALIB_I * DPOW * KSI * KINT )   VREF = 1.18 from datasheet AI = 16 from datasheet CALIB_i = 0.875 from datasheet DPOW = removed KSI = Rshut = 0.05 ohm when I ca...

Gz by Senior
  • 1393 Views
  • 2 replies
  • 0 kudos

MKI109V3 with MKI197V1 problem

Hi,I have asked this question in community also but no answer till now.I have got below devices as one of your colleague offered me via email.I have a MKI109V3 and one MKI197V1.I have downloaded the related tools&software of MKI109V3 then I opened th...

spark by Associate II
  • 1475 Views
  • 2 replies
  • 0 kudos

LIS2DH12 bandwith and aliasing

Hello, is there any kind of anti aliasing filter in the LIS2DH12 the datasheet is not clear to me. In the datasheet of the LIS2HH12 there are some settings according to analog aliasing filters. So is this filter not present in the LIS2DH12 or only su...

THart.14 by Associate II
  • 1135 Views
  • 1 replies
  • 0 kudos

Resolved! L3GD20H raw value conversion

How does one convert:Raw angular rotation data to DPSRaw temperature sensor readings to degreesThanks :grinning_face: