MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MotionAW does not leave MAW_STATIONARY

Hi,​Im trying to evaluate MotionAW on a BlueCoin dev kit. After a few seconds MotionAW_Update returns AMW_STATIONARY (before that it returns MAW_NOACTIVITY), and after that the activity doesnt seem to change. What am I doing wrong?For all I can see t...

HSmed by Associate
  • 835 Views
  • 0 replies
  • 0 kudos

Resolved! VL53L1X RangeStatus No Update problem

Hi!I want use an VL53L1X sensor for our project. I "ported" to original ST api to TI chip and TIRTOS. But I cant measure any distance. Now I just want to try the sensor, so I using "polling" method. But when I call a GetMeasurementDataReady function...

RSzil by Associate
  • 2052 Views
  • 2 replies
  • 0 kudos

VL53L0X - how to run on stm ?

Recently I've bought vl53l0x sensors and I'm struggling 2 weeks to run it on my stm. I've bought pololu sensor and i want to connect it to Nucleo board. There is no explanation how to achieve this. There are only tutorials for specific boards and boa...

DGo�? by Associate
  • 1051 Views
  • 1 replies
  • 1 kudos

HTS221 blocks SDA line

I tried to connect the HTS221 to the ATtiny816 via the I2C bus. The data availability survey was conducted 2 times per second:if ((HTS221_GetCTRL_REG2() == 0) && ((HTS221_GetStatus() & 0x03) == 0x03)) {         HTS221_GetData(&HTS221_Rx_buf); ...

Lehman by Associate II
  • 1795 Views
  • 4 replies
  • 0 kudos

LIS331HH Frequency Response and Max acceleration detection Question

What is linearity with frequency like? I guess the sensor has a roll off at some frequency due to its mechanical characteristics?The block diagram suggests no analogue filter between the mux and A/D. How does the system deal in practice with vibratio...

JLitt by Associate II
  • 1171 Views
  • 1 replies
  • 0 kudos