cancel
Showing results for 
Search instead for 
Did you mean: 

Using VL53L0X with STM32L476 Nucleo64?

va vai
Associate
Posted on March 05, 2018 at 16:43

Hi,

I am a novice trying to work on some sensors by connecting them to the STM32L476 nucleo 64 board. Currently I am trying to use the Time of flight sensor, VL53L0X breakout board, by connecting it at the I2C pins on the nucleo 64.

Also, I am using system workbench to run the generated code.

I am unable to understand as to how to include the drivers/Api for the sensor into the project (created using Cube Mx and the system workbench) so that I can use it to access the sensor. Is there a simple process that anyone can explain? Even hints in the right direction would be really helpful. Also it would be great if anyone could point me to links showing ckt connections between a STM32 nucleo and TOF sensor.

Thank you for the help and have a nice day!!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
helmi haddad
Associate II
Posted on June 20, 2018 at 10:19

hello , can you send to me your example please ?

DNowi
Associate

I don't have an answer but I'm having a massively hard time trying to figure out how to use the API package that is provided. If I find an answer I will do my best to post it.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.