MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need help getting initialized with MSP430F5529 to lsm303agr using STMems_Standard_C_Divers

 P4SEL |= 0x06;              // Assign I2C pins P4.1, P4.2 to USCI_B1 UCB1CTL1 |= UCSWRST;           // Enable SW reset UCB1CTL0 = UCMST + UCMODE_3 + UCSYNC;   // I2C Master, synchronous mode UCB1CTL1 = UCSSEL_2 + UCSWRST;      // Use SMCLK UCB1BR0 =...

JBonn by Associate III
  • 926 Views
  • 1 replies
  • 0 kudos

Is it possible to change the STEVAL-IDP005V1-GUI software files?

Hello everyone,I am conducting some tests with the STEVAL-BFA001V1B and STEVAL-IDP004V1 evaluation kit together with the STEVAL-IDP005V1 GUI software available on STSW-BFA001V1.But I need to make some changes in the STEVAL-IDP005V1-GUI software, the ...

Hertzing by Associate II
  • 1699 Views
  • 4 replies
  • 0 kudos

Resolved! STEVAL-MKI109V3 DfuSe update issue, no available DFU Device

Hello, I installed the latest driver version Unico 8.0.0. Now my board is shown in the decive manager.Ready to use.. Everything looks good.Now I am trying to update the FW in the STEVAL-MKI109V3 board. First I pressed the BT2 Button and pluged the US...

Chris0815 by Associate II
  • 1432 Views
  • 2 replies
  • 0 kudos

Generate Interrupt on horizontal rotation using LIS3DH

Hi,I have a jar lid which is equipped with LIS3DH accelerometer. The accelerometer is placed in the PCB such that the top layer of LIS3DH will face the sky in normal position. The jar has a groove for holding the lid and we need to put the lid in th...

IThom.5 by Associate II
  • 2473 Views
  • 5 replies
  • 0 kudos

LIS2DH12TR 1. Calibration 2.sleep mode and wake-up mode detail explanation & 3.example code for interfacing with the CC1310 (SCS and CSS)

Hi,I have couple of question on LIS2DH12TR .I'm trying to interface with CC1310 Custom Board.1. As per the data sheet it says it doesn't need any manual calibration since factory calibration already done.( Previously have used MPU6050 didn't know m...

LN by Associate II
  • 1142 Views
  • 1 replies
  • 0 kudos

IIS2DLPC Data Rate Accuracy

The actual sampling rates deviate from the published. For example and ODR of 25Hz is actually ~30Hz. Is this typical? We did not notice this on the IIS2DH part. I expected some variance from the desired rate, but is every device going to vary this mu...

iaeinfach by Associate III
  • 1847 Views
  • 3 replies
  • 0 kudos