MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sensor tile soldering problem

Any known issues with soldering a STLKT01V1 (sensor tile ) to the small carrier board?I did this, and now it does not work (no jtag) it worked prior with large boardI do not want to destroy a 3rd board!

delli by Associate II
  • 1417 Views
  • 2 replies
  • 0 kudos

LSM6DSO inclinometer

Hi,I was playing around with Unico and I saw it has an inclinometer function. Is the code for that window available:? I tried an implementation with Kalman filter, but the Unico seems to show the angles much better.Regards,Gabriel

LSM6DSL selftest thresholds

Hi, we are using LSM6DSL, and we are developing the self-test procedure. The Self-test algorithm for LSM6DSL is described in AN5040 Application note, but we don't know the values |min(ST_X)|, |max(ST_X)|,|min(ST_Y)|, |max(ST_Y)||min(ST_Z)|, |max(ST_Z...

massimo2 by Associate II
  • 1175 Views
  • 2 replies
  • 0 kudos

STEVAL-WESU 1 design files

Hello,I'm developing a product starting from the WESU eval product. I see on the webpage the pdf with the schematics and the gerber files for production, but unlike other eval boards I cannot find the design project. Could you please provide it? Than...

LSM6DS3 SPI Communication Problem

I tried to work with mbed LPC1768 and LSM6DS3-Dev-Board from Sparkfun.The connections:uC - LSM6DS3VOUT 3V3 regulated Out - 3V3GND-GNDSCLK-SCLMOSI-SDA (SPI SDI)MISO-SA0CS-CSThe Code:#include "mbed.h"   Serial pc(USBTX,USBRX); SPI spi(p11, p12, p13); /...

ogris by Associate II
  • 6232 Views
  • 6 replies
  • 0 kudos

CTRL_REG1 configuration timing

I was trying to debug a driver written by another developer and I noticed they setup CTRL_REG1 through CTRL_REG6 with a 5ms delay between each register write. I asked the developer the reason for the delays and they said that if the registers were wr...

JBald by Associate
  • 709 Views
  • 0 replies
  • 0 kudos

LIS3MDL X Axis freezes at 32764. Why?

My LIS3MDL eCompass IC output always reads (X=32764) for the X axis.Axis y and z seem to read ok, with changing values during operation.Why is this occurring?The first day of use the LIS3MDL worked OK, with X,Y,and Z axis having unique and changing v...

KHueb by Associate II
  • 1351 Views
  • 3 replies
  • 0 kudos

Sample product

Hello,i want to order a sample product iis2mdc because i don't find it available in any store.In my order it says "total price $0.00" and "subtotal: $0.00"but in the field "shipping cost: Estimate" in my country(Greece) has a shipping cost of $37.00....

0690X000008aGVxQAM.bmp 0690X000008aGY8QAM.bmp
ASIGA by Associate
  • 1064 Views
  • 2 replies
  • 0 kudos