cancel
Showing results for 
Search instead for 
Did you mean: 

SelfTest functionality followed Application Note AN-5005, using LIS2DH12. What is the MIN ST_X and MAX ST_X mean in the Application note AN5005?

VLaks
Associate

LIS2DH12 is Configured with BDU=1, Normal Mode, FS=2G. While doing the below step after collecting the data, in non-selftest mode and self mode. We followed the steps detailed in the Application Note AN-5005 and each axis has to be checked as below

|MIN(ST_X)| <= OUTX__ST - OUTX_NOST<= |MAX(ST_X)|. similarly for y and z axis is mentioned.

1) Does this MIX(ST_X) and MAX(ST_X) Refer to table 4 Mechanical Characteristics in the Datasheet the Self Test Low is expected to be 17 and Max to be 360

2)what is this value against which should the data be compared.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0