MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MotionFD and SensorTile compatibility

Hello ST Community,I would like to ask if the (1)SensorTile and/or (2)SensorTile.box are compatible with the MotionFD library?According to the MotionFD user manual, the library uses Accelerometer and Pressure Sensor data to detect a fall, which both ...

DIM by Associate II
  • 1142 Views
  • 1 replies
  • 0 kudos

LIS3DH don't send ACK at 9th clock pulse

I am using LIS3DH accemelator to acuqire gravity data. The MCU is NXP MKL16. LIS3DH's pin8 CS is set to high level to communicate with I2C protocol, and pin7 SA0 is set to connect to GND. The SCL and SDA pins are pull up with 4.7K resisttors. After ...

0690X000009Yv7cQAC.png

LIS2DH12 INT1 not sending interrupts

I am trying to configure the LIS2DH12 to send free-fall interrupts but I have not been able to successfully see any interrupts. Here are the register values that I set:CTRL1(0x20) = 0x47 (ODR = 50hz, XYZ enabled)INT1_THS(0x32) = 0x40INT1_DUR...

RKrei by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

LSM6DSOX: 3 vs 4 wire SPI configuration

Hello, this should be a basic question but I am pretty new in this field. What are the core difference between a 3 and a 4 wir SPIe configuration for LSM6DSOX? Apart from electrical connection, is there any difference in Firmware design, capabilities...

ANist by Associate III
  • 2122 Views
  • 3 replies
  • 0 kudos

LIS2DH power consumption with 1 axis enabled?

We're evaluating the LIS2DH (and -DE) for a very low-power project, and every uA is precious. We only need readings from one axis, so I am curious as to whether disabling the other two axes would result in power savings. I've tried measuring it her...

eggs by Associate
  • 1405 Views
  • 1 replies
  • 0 kudos