cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L0X MBED libraries

Julien NGUYEN
ST Employee

Where to find the VL53L0X MBED libraries ?


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Julien NGUYEN
ST Employee

​You can find the VL53L0X MBED here below

https://os.mbed.com/teams/ST/code/VL53L0X/


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks for the link, but is there a way to make it compatible with the LPC1768?

The library uses other libraries, like the X_NUCLEO_COMMON, ST_INTERFACES and STMPE1600. Since the LPC1768 doesn't use the STMPE1600, is it possible to send a NULL instead of a STMPE1600 object? Wait, I didn't realize there was a VL53L0X constructor without the STMPE1600 object

Is it possible to provide example programs with this library?

I guess not then, alright