MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use PDM MEMS microphone on PB8 (MCLK) with STM32WBxx

I am using the MEMSMIC1 Microphones_Streaming example (https://www.st.com/en/embedded-software/x-cube-memsmic1.html) with the STM32WBxx chip. I am trying to change the clocking pin from PB13 to PB8 to use the example with custom hardware.I am trying ...

FFlet by Associate II
  • 1002 Views
  • 1 replies
  • 0 kudos

Resolved! LSm303agr power-down

Hi guys,I'm using for first time LSm303agr sensor and I have a question about low-consumption of the sensor.Reading the Electrical characteristic I see that the sensor can achieve a low consumption of 2uA but I don't know what registers can do it.I u...

0690X000009Z1r3QAC.png
MM.10 by Associate II
  • 2886 Views
  • 5 replies
  • 0 kudos

blog.st.com

We’ve just announced the launch of a new sensor unit called SensorTile.box. It is a flexible IoT Plug and Play module to jumpstart sensor-to-cloud IoT applications.Find out what you can do with the SensorTile.box by reading our blogpost at  https://b...

0690X000008BOslQAG.jpg

Resolved! Problem with L3G4200 Sensor using I2C

I have a problem interfacing with L3G4200 using I2C on STM32F469 Discovery. Here is my code to config the I2Cvoid I2CConfig(void){ I2CHandle1.Instance = I2Cx; I2CHandle1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; I2CHandle1.Init.ClockSpeed = ...

Resolved! Microphones streaming through I2S

Hi,I'm trying to implement the streaming of two MEMS microphones via I2S.Following some examples provided by ST, I was able to implement the acquisition of the two microphones: I obtain a 32 samples buffer PCM every 1 ms (left and right channel).Now ...

Fib by Associate II
  • 1974 Views
  • 2 replies
  • 0 kudos

VL53L1X NON_BLOCKING measurement

Hey,I am using the vl53l1x on a raspberry pi with python (pimoroni library). However, to my knowledge and experience, by default the waiting method for measurement data is BLOCKING. So in Python the get_distance() function takes about as much time as...

VL53L1X test with a foggy area and distance impacted!

Posted on June 12, 2018 at 10:28Description:We use 4 -VL53L1X sensors in our product and we have a closed box (rectangular shape), in which we place a foggy stuff for a worst air condition to see object distance impact or not.Before the foggy stuff ...

0690X0000060LDrQAM.png
leo su by Associate II
  • 1970 Views
  • 2 replies
  • 0 kudos

Floating point implementation type for MotionAC Library

Hi everyone, i'm working on a project which i use Atollic TrueStudio as IDE and NUCLEO-F303RE as evaluation board. I was inplementing floating point as "hardware" before i decided to use MotionAC library but after adding library to my project i could...

N ORhan by Associate III
  • 866 Views
  • 0 replies
  • 0 kudos