MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

.

FPira by Associate
  • 627 Views
  • 0 replies
  • 0 kudos

Trouble getting sensortile working with small cradle

Not sure if I'm in the right place for this question, but I recently started using the sensortile development kit for a class/project. I've done all the tutorials with the sensor mounted to the expansion cable. However, now my project requires the ...

JCrow by Associate II
  • 2130 Views
  • 5 replies
  • 0 kudos

The interface firmware FAILED to reset/halt the target MCU FAIL.TXT message on my STEVAL-IDP005V1. How do I fix this?

I have connected STEVAL-IDP005V1 sensor board (it has an STM32F469AI ARM® Cortex®-M4 32-bit MCU on it) to the ST-LINK/V2-1 programmer/debugger on stm32 NUCLEO-F401RE board via an adapter board STEVAL-UKI001V1. When I connect the USB cable to the PC a...

Chandu by Associate II
  • 1696 Views
  • 2 replies
  • 0 kudos

SW or pre recorded examples for SensorTile.BOX

Hy,I've just acquired the new sensorTile BOX and try to discover is capabilities (who are wery perfect for me) but i encoundered some issues with battery. It's seems to be impossible to have the status (unknown) and the red light blinking fastly when...

[SOLVED] Reading temperature sensor on LIS2DE12 via I2C

I have implemented in our product a LIS2DE12 sensor. I would like to read the temperature register via I2C.In order to do this I setup the following register:at start-up:-check WHO_AM_ I register (0x0Fh) which correctly reports 0x33h (so I2C bus and ...

SensorTile Kit (STLKT01V1) does not turn on

Purchased a SensorTile Kit (STLKT01V1) which stopped working after a day.Removed the contents from the package, placed the sensortile on the large cradle, powered it using USB power supply from my laptop and it worked. The Orange LED flashed, I was a...

TRobi by Associate
  • 1823 Views
  • 3 replies
  • 0 kudos

Power consumption LIS3DSH

Hi allCan I have a table of power consumption for LIS3DSH in different sampling rate?Kind RegardsReza

MNaee by Associate
  • 1222 Views
  • 2 replies
  • 0 kudos

Get data from NUCLEO-F767ZI with Unicleo-GUI.

I have NUCLEO-F767ZI with plugged X-NUCLEO-IKS01A2 and some DIL24 evaluation sensors. Where can I get example firmware for NUCLEO-F767ZI to get data from DIL24 sensors with Unicleo-GUI?Thank you!

DLapt by Associate
  • 1437 Views
  • 2 replies
  • 0 kudos