MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

"Fusion" icon not showing in Unico

Hi.I am working on evaluation with STEVAL-MKI210V2K. I use Unico to get sensor data, however what I really want is post-fusion data. Looking at other forum questions, it seems like Unico gives a "fusion" option on the left vertical tab. I don't have ...

ariy_0-1737647049593.png
ariy by Associate
  • 733 Views
  • 1 replies
  • 0 kudos

ism330dhcx i2c get accel_x,y,z and heading calculation issue

Hi,     We are use openWRT and  ism330dhcx and LIS2MDLTR  on board.  The ko driver   has been created and  insert into kernel . When read data from  /sys/devices/platform/i2c_gpio@0/i2c-0/0-006a/iio:device2/in_accel_XXXX,   We has found the Z value i...

arprip by Associate
  • 349 Views
  • 1 replies
  • 0 kudos

LSM6DS3 FIFO data corruption on random basis.

Hi everyone! I am using LSM6DS3 in a very simple setup: For the debugging purposes I am only using accelerometer, ODR is set at 416Hz, fifo is enabled in continuous mode and set at the same freq, no decimation. Only XL data is set to be stored in fif...

oversc0re by Associate II
  • 1924 Views
  • 5 replies
  • 2 kudos

Enabling FIFO on LSM6DSOX

Hi,  I'm trying to get the FIFO working on the LSM6DSOX on a custom board with a silicon labs microcontroller, communicating both through SPI. I have checked the application note at https://www.st.com/resource/en/application_note/an5272-lsm6dsox-alwa...

amarco by Associate II
  • 5352 Views
  • 15 replies
  • 1 kudos

Resolved! Anyone have v1.3.1 MEMS-STUDIO for download

Hi,We've been working on a project using v1.3.1 of MEMS Studio, but I've had to use a new laptop and it doesn't have this installed. Unfortunately, when I go to the downloads page I can only see v1.4.1 of MEMS Studio and it's forcing me to upgrade th...

SFowler by Associate II
  • 1717 Views
  • 8 replies
  • 0 kudos

LSM6DSV16B voltage spikes on SPI data out

I am trying to read the data of the accelerometer and gyroscope of the LSM6DSV16B with an FPGA. I build a 4 wire SPI-Interface. I am able to write data to the chip and the chip is capable to give data out. But sometimes the output of the chip gets dr...

Screenshot 2025-01-13 092026.png
flx by Associate
  • 457 Views
  • 2 replies
  • 0 kudos

Testing pressure sensors

Hello,I am working on water ingress application experiment, and I want to know how to evaluate different pressure sensors to figure out which one is best for me? Since this application involves water, I think a water proof option would be good. But w...

Lsm6ds3tr_c interrupt not triggered

I use the official lsm6ds3tr-c-pid driver,Here is the code I initialized:  u8 who_amI = 0; lsm6ds3tr_c_device_id_get(&dev_ctx, &who_amI); if (who_amI != LSM6DS3TR_C_ID) { printf("lsm6ds3tr_c_device_id_get err,%d,%d", who_amI, LSM6DS3TR_C_ID); } pri...

hanjie by Associate
  • 368 Views
  • 1 replies
  • 0 kudos