cancel
Showing results for 
Search instead for 
Did you mean: 

Anyone have v1.3.1 MEMS-STUDIO for download

SFowler
Associate II

Hi,

We've been working on a project using v1.3.1 of MEMS Studio, but I've had to use a new laptop and it doesn't have this installed. Unfortunately, when I go to the downloads page I can only see v1.4.1 of MEMS Studio and it's forcing me to upgrade the firmware, which I don't want to do as all our testing & benchmarking has been based on a specific configuration.

Does anyone have, or can you point me to, the older version of the application? ST don't seem to have an archive of older builds anywhere and their support team has been unable to help.

Thanks,

Simon

1 ACCEPTED SOLUTION

Accepted Solutions
liaifat85
Senior III

If your organization has previously used MEMS Studio v1.3.1, it's possible that the installation files are stored on internal servers, backup systems, or within your team's shared resources.

View solution in original post

9 REPLIES 9
liaifat85
Senior III

If your organization has previously used MEMS Studio v1.3.1, it's possible that the installation files are stored on internal servers, backup systems, or within your team's shared resources.

Yes, I thought that too, but it's a fairly small team and nobody seems to have the installation media. We are looking at backups, but this will take some time. I was hoping ST would have an archive, but it seems not :O(

Federica Bossi
ST Employee

Hi @SFowler ,

Version 1.3.1 has not been released, the official version is 1.3.0 which we can share with you.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks, Federica, that would be great. What is the best way for you to share the download with me?

Simon

Hi @SFowler ,

if you give us your email address we will contact you by sending you the version  1.3.0 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Brilliant! My email is sif@simcorp.com.

The help is much appreciated.

Thanks for the offer of help. However, we have managed to locate the version of MEMS-Studio that we wanted.

Will close this post.

Can you share with me too, my email id is muzzu1318@gmail.com

ephraim-s
Associate II

can I get 1.8.2?

I need is since 2.2.0 doesn't recognize any option with my ISM 330 evaluation sensor.

 

ephraims_0-1769595249931.png

Thanks,

Ephraim