MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! lsm6dso and lsm6dsox SW detection

We use two types of sensors for our dev: lsm6dso and lsm6dsox. It is necessary to detect the type of sensor SW (without opening the device). And it's difficult, because adress (we use i2c) is the same, Device Identification (Who am I) is the same for...

YRakh.1 by Associate II
  • 4049 Views
  • 6 replies
  • 0 kudos

www.st.com

Free massive open online course (MOOC) with hands-on exercisesLearn to design with ST's newest and most advanced motion and environmental sensors with an easy-to-use STM32Cube development ecosystem.This free, self-paced video course features hands-on...

0693W000001rfQPQAY.png

How do I flash original Sensortile mobile app code?

When I received the Sensortile chip, it had the mobile app code flashed on it.I was working on developing on the Sensortile chip, so I flashed my own .bin file onto the chip using ST-LINK Utility.Now I want to revert back to the mobile application co...

FLee.1 by Associate
  • 1133 Views
  • 1 replies
  • 0 kudos

Is there another driver to get BOTH data buffer instead of VL53L1_GetRangingMeasurementData()? This one ONLY returns one result then I can't calculate a "shift" by using just one sensor.

VL53L1_GetRangingMeasurementData() ONLY returns data[0] buffer as result. It means that I will get just the result of ONLY one of the two sensor in the matrix. I'm trying to implement your "people counter" posted on youtube (https://www.youtube.com/w...

SLomb.1 by Associate
  • 763 Views
  • 0 replies
  • 0 kudos

How to completely power down the lsm9ds1?

I'm using the lsm9ds1 as part of a bought module - the arduino nano 33 ble - which can achieve very low power (micro amps) in a power down mode. However, If I initialize and read accel and gyro data from the IMU, afterwards I can't find a way to get ...

PRebo.1 by Associate II
  • 1050 Views
  • 0 replies
  • 0 kudos

Battery level using bluepy and FP-SNS-ALLMEMS2

HelloI had download the firmware FP-SNS-ALLMEMS2 on my STEVAL-MKSBOX1V1. From de app I can read the batery level, and I want to do the same with my raspberry and using bluepy. I have a script where I read the temperature and humidity values, so I wan...

NMart.1 by Associate III
  • 1224 Views
  • 1 replies
  • 0 kudos