MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X long range mode

I am using VL53l0x and I want to measure distances of 2 meters but I don't find the function to configure long range mode.

Mcabe.1 by Associate II
  • 742 Views
  • 0 replies
  • 0 kudos

Set LIS2DH12 in power down mode

Hello ST Community,My application involves nRF52 series processor which interfaces with LIS2DH12 via SPI and I am trying to reduce the power consumption as much as possible when the processor is in sleep mode. I understand that, as soon as power is a...

AB.4 by Associate II
  • 2067 Views
  • 2 replies
  • 0 kudos

Algobuilder IIR Filter a10/a20 coefficient

Hi!I am using the IIR function block in Algobuilder. In the UI I can enter the coefficients manually or use a file. The implementation uses the CMSIS functions Biquad Cascade IIR Filters Using Direct Form I Structure (void arm_biquad_cascade_df1_init...

DWind.1 by Associate III
  • 1263 Views
  • 1 replies
  • 0 kudos

Export raw accelerometer- and FFT-values from Unicleo

Hi!I have a Nucleo board and use the FFT example that comes with Algobuilder. It shows all the data and the results from FFT in the separate window. I would like to export all the data (accelerometer values, FFT results, peaks, etc). It works with ac...

0693W000001scykQAA.jpg
DWind.1 by Associate III
  • 988 Views
  • 1 replies
  • 0 kudos

LSM6DSL does not respond well anymore

I was testing the LSM6DSL, at first 10 versions of my firmware, the sensor is working fine, I was able to read and write to its register. Now it does not work, reading the WHO_I_AM register gives different value than 0x6A. I hope you can help me.

JBrio.1 by Associate II
  • 1704 Views
  • 2 replies
  • 0 kudos