MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! lsm6dsr driver fix?

Hello,One of my previous post the driver for the sensor lsm6dsox hub mode 2 configuration, I have written that the function lsm6dsox_sh_read_data_raw_get was not working correctly. I managed to fix it.Now I see someone fixitNow I'm using lsm6dsr and ...

0693W000004IVG2QAO.png
suads by Associate III
  • 1645 Views
  • 2 replies
  • 0 kudos

Resolved! Motionfx problems with quaternions

Hello I have previous implemented the motionfx to get quartenions using lsm6dsl and lsm303agr over i2c, and everything was working great. Now I changed the sensor lsm6dsl with lsm6dsox who is communicating over spi with stm and lsm303agr in mode2(spi...

suads by Associate III
  • 2726 Views
  • 3 replies
  • 0 kudos

APIs DSH-PREDMNT

Hello,I am using a STEVAL-STWINKT1 connected to ST cloud: DSH-PREDMNTI want to increase the number of devices and time of use, is this possible? what is the procedure to do it?If not, do you provide the APIs to implement it in my own dashboard?can t...

a123 by Associate II
  • 10464 Views
  • 15 replies
  • 1 kudos

SensorTile.Box python get acc events

Hi,i'm trying to send acc events e.g. single tap, double tap via bluetooth to python SDK (BlueSTSDK), but i have no ide how to do it. I can send any other feature like acceleration and gyroscope data.

TNie.1 by Associate
  • 1196 Views
  • 2 replies
  • 0 kudos

An entire volume on the SensorTile.box from Elektor

"Sensors are quintessential devices used extensively in nearly all microcontroller-based applications. In many applications, the designer chooses the sensors to be used as external devices and connects them to the target processor. [...] This book is...