cancel
Showing results for 
Search instead for 
Did you mean: 

Hts221 how long does the heater have to be ON to clear condensation

RSoto.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

HI @RSoto.1​ ,

the exact time of the condensation recovery would depend on the "condensation level" on the sensor.

Assuming the maximum condensation, I can share you an average characterization results:

  • Example: Fridge. Max condensation to ambient 68%:
    • without heater --> 800 seconds
    • with heater on --> 10 seconds

Please note also that the amount of current flowing in the heater depends on the Vdd, and is proportional to the RH% reduction in a constant timeframe. For example, 1-minute heater ON at Vdd=3.3V drops the humidity of -23rH, while at Vdd=1.8V the drop is -8rH, same timeframe.

-Eleon

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

HI @RSoto.1​ ,

the exact time of the condensation recovery would depend on the "condensation level" on the sensor.

Assuming the maximum condensation, I can share you an average characterization results:

  • Example: Fridge. Max condensation to ambient 68%:
    • without heater --> 800 seconds
    • with heater on --> 10 seconds

Please note also that the amount of current flowing in the heater depends on the Vdd, and is proportional to the RH% reduction in a constant timeframe. For example, 1-minute heater ON at Vdd=3.3V drops the humidity of -23rH, while at Vdd=1.8V the drop is -8rH, same timeframe.

-Eleon

Eleon BORLINI
ST Employee

Hi @RSoto.1​ ,

do you have any feedback about your request?

-Eleon