cancel
Showing results for 
Search instead for 
Did you mean: 

IIS2ICLX inclination

gio926
Associate

Hello, I'm looking for a very high precision inclination sensor. I found this IIS2ICLX. I have some questions on the specifications.

1) What is the repeatability of the device?

2) From the spec sheet, it might seem like the repeatability of the device is 0.075mg but it's unclear. If that is the spec, can you help me in converting this to degrees?

3) Are there other devices that have a higher repeatability?

 

Thanks

2 REPLIES 2
Federica Bossi
ST Employee

Hi @gio926 ,

What do you mean by repeatability?

0.075 mg/°C is the stability over temperature.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hii mam,i am also looking for high precision inclination ic is IIS2ICLX this ic will suitable for my requirment resolution 0.001 to 0.005 degree and accuracy sholud be 0.01 degree .if not please tell any other ic that meets my requiments...Waiting for your positive reply