MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X API Status: -6 : Range error. I developed a little instrument using VL53L0X to measure a distance ranging from 30 to 200 mm. We assembled 200 pcs and on 50% of them I get the error above, while the remaining 50% work fine. Anybody can help me?

API Status: -6 : Range error ===============================//my code.....  if(Status == VL53L0X_ERROR_NONE)  {  //   printf ("Call of VL53L0X_StaticInit\n");    Status = VL53L0X_StaticInit(pMyDevice); // Device Initialization    print_pal_error(Stat...

GBern by Associate
  • 1475 Views
  • 0 replies
  • 0 kudos

Resolved! Hello everyone I downloaded the API for VL53L3 range sensor. I try to compile the API with Eclipse but the file ranging_sensor_comms.h is missing (included in vl53lx_platform.c). What is this file? Where is this file documented? Thank you for your help

Ultimately, I would like to know where I2C commands are described in order to re-write my own I2C R/W function according to my hardware. First I woud like to play with the entire API to get familiar with it. The file ranging_sensor_comms.h is not inc...

Ben1 by Associate III
  • 6942 Views
  • 10 replies
  • 0 kudos

VL53L3CX API : WaitDeviceBooted returns 1??

Hi everyone. I try to integrate VL53L3CX range sensor in an applicaction using nRF microcontrollers. I am using the API 1.1.4. I would like to test a I2C read first, so I edited the function VL53LX_ReadMulti() in file vl53lx_platform.c as follow :VL5...

0693W00000593ZqQAI.png 0693W00000593ZgQAI.png
Ben1 by Associate III
  • 1682 Views
  • 1 replies
  • 0 kudos

HardFault once calling MotionFX_propagate()

my mcu is STM32F730R8Txsensor: LSM9DS1use CubeMx gen code, with Makefile(under linux env)I use lsm9ds1_reg.c as sensor driver fetch raw data, and it worked fine.then, do the following as MotionFX lib documents:MotionFX_initialize()MotionFX_getKnobs(&...

MMa.1893 by Associate III
  • 10758 Views
  • 23 replies
  • 0 kudos

Resolved! Is the LSM9DS1 accelerometer sensitivity right for the 16G?

I am using the IMU LSM9DS1. However, when developing the library for communicating with the IMU and reading the accelerometer values, I noticed something odd.According to the datasheet, the sensitivity of the accelerometer is given by: which normally...

0693W000005Bc3ZQAS.jpg
MSanc.1 by Associate II
  • 2675 Views
  • 7 replies
  • 0 kudos

how to differentiate between different detections(freefall, motion and tampering detection)when they are configured on the same interrupt?

i am currently working using LIS2DH12TR sensor, on which i had configured the below detections on interrupt 1, how to differentiate between different detections(freefall, motion and tampering detection)when they are configured on the same interrupt?w...

Mnago.1 by Associate II
  • 1321 Views
  • 1 replies
  • 0 kudos