2025-03-06 6:34 PM
I am making a simple inclinometer using IIS2DLPC. The 'Zero-g offset change vs. temperature' of IIS2DLPC is specified as a maximum of ±1mg/℃, but some of the boards I made have reached 2.93mg/℃.
Some have relatively good values of 0.3-0.4mg/℃, while others have values of 0.8-1.6mg/℃, so the characteristics vary.
2.93mg/℃ is the worst value evaluated.
Since most of the units can be measured cleanly, I think that it is not a problem with the circuit board, but some external factor is at work. Please let me know if there are any possible factors.
Note that the measurements are taken only on the printed circuit board, without being assembled into a case.
2025-03-07 2:53 AM
Hi @t-susaki ,
You may see different values depending on the part because 1mg is just a typical value that takes into account piece-to-piece variability.
However, 2.93mg/℃ is a little too high a value. Could you please share the settings with which you acquire the data? In what temperature range are you testing?
Thanks
2025-03-09 4:56 PM
Thank you for your reply.
I have set the registers as follows.
CTRL1=00000100
CTRL2=00001100
CTRL3=00000000
CTRL4_INT1=00000100
CTRL5_INT2=00010000
CTRL6=11000100
CTRL_7=10100000
FIFO_CTRL=00000000
The temperature range is +20°C to +40°C.
If there are any errors in usage, please let us know.
2025-03-12 5:30 PM
I recently responded to a question from you, but have not yet received a reply.
What can you tell us from the following information?
I have set the registers as follows.
> CTRL1=00000100
> CTRL2=00001100
> CTRL3=00000000
> CTRL4_INT1=00000100
> CTRL5_INT2=00010000
> CTRL6=11000100
> CTRL_7=10100000
> FIFO_CTRL=00000000
> The temperature range is +20°C to +40°C.
> If there are any errors in usage, please let us know.
2025-03-13 3:28 AM
Hi @t-susaki ,
I am a little bit confused. In CTRL1 you write 00000100 so you are setting the high performance mode but the sensor is in PD?
2025-03-13 5:00 PM
My apologies. I did not explain myself well enough.
Our product is battery-powered, so when it is not measuring, it is in power-down mode to reduce power consumption.
When measuring, the CTRL1 register is rewritten to '01010100' and returned to '00000100' when the measurement is finished.